Hello:
I have followed the guide "HowttoFlash - dcdcLighting" to allow the GUI to work properly but I am having difficulty with my connection to the Target(F28035). All the jumpers and switches are configured correctly.
"Rebuild the Project" goes fine but when I try to do the "debug the active project" I get the error "An error was encountered when attempting to load the program". In the console I get the following:
C28xx: Flash Programmer: Missing Flash Programming Settings
C28xx: Flash Programmer: Error erasing Flash memory.
C28xx: Flash Programmer: Missing Flash operation option. Operation cancelled.
C28xx: Trouble Writing Memory Block 0x3f6f82 on Page 0 of Length 0x53
Cannot write to target.
I have CCS Version4.2.1.00004 and I have verified that I have the lastest Control Suite V1.9 software for the DC/DC LED Lighting Kit. I have also verified that the drivers for the xds100v1 USB Emulator are the most current. My computer is allocating COM port 18 for the Emulator.
Any help with this matter is greatly appreciated in advance.
Thank you