Other Parts Discussed in Thread: C2000WARE
I need Guidance for using CLAsin() function. Though I referred CLA_MATH_LIB_UG.pdf, I have the following questions
1. My program showed warning to create CLAMathTable untill i add "F2837xRevB_c1bootROM_CLADataROMSymbols_fpu32.lib" with first priority. After adding, my warnings vanished and still CLAsin() function is not working in my cla task. I am using Control card so i am using RAM in my cmd. Should I modify my cmd file?
below is my cmd file
// The user must define CLA_C in the project linker settings if using the // CLA C compiler // Project Properties -> C2000 Linker -> Advanced Options -> Command File // Preprocessing -> --define #ifdef CLA_C // Define a size for the CLA scratchpad area that will be used // by the CLA compiler for local symbols and temps // Also force references to the special symbols that mark the // scratchpad are. CLA_SCRATCHPAD_SIZE = 0x100; --undef_sym=__cla_scratchpad_end --undef_sym=__cla_scratchpad_start #endif //CLA_C MEMORY { PAGE 0 : /* BEGIN is used for the "boot to SARAM" bootloader mode */ BEGIN : origin = 0x000000, length = 0x000002 RAMM0 : origin = 0x000123, length = 0x0002DD RAMD0 : origin = 0x00B000, length = 0x000800 RAMD1 : origin = 0x00B800, length = 0x000800 /* RAMLS4 : origin = 0x00A000, length = 0x000800 */ /* RAMLS5 : origin = 0x00A800, length = 0x000800 */ RAMLS4_5 : origin = 0x00A000, length = 0x001000 RESET : origin = 0x3FFFC0, length = 0x000002 PAGE 1 : BOOT_RSVD : origin = 0x000002, length = 0x000121 /* Part of M0, BOOT rom will use this for stack */ RAMM1 : origin = 0x000400, length = 0x0003F8 /* on-chip RAM block M1 */ // RAMM1_RSVD : origin = 0x0007F8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ /* RAMLS0 : origin = 0x008000, length = 0x000800*/ EPWM1ISR_LS0 : origin = 0x008000, length = 0x000050 ECAP1ISR_LS0 : origin = 0x008050, length = 0x000050 RAMLS0 : origin = 0x080A0, length = 0x000760 RAMLS1 : origin = 0x008800, length = 0x000800 RAMLS2 : origin = 0x009000, length = 0x000800 RAMLS3 : origin = 0x009800, length = 0x000800 RAMGS0 : origin = 0x00C000, length = 0x001000 RAMGS1 : origin = 0x00D000, length = 0x001000 RAMGS2 : origin = 0x00E000, length = 0x001000 RAMGS3 : origin = 0x00F000, length = 0x001000 RAMGS4 : origin = 0x010000, length = 0x001000 RAMGS5 : origin = 0x011000, length = 0x001000 RAMGS6 : origin = 0x012000, length = 0x001000 RAMGS7 : origin = 0x013000, length = 0x001000 RAMGS8 : origin = 0x014000, length = 0x001000 RAMGS9 : origin = 0x015000, length = 0x001000 RAMGS10 : origin = 0x016000, length = 0x001000 // RAMGS11 : origin = 0x017000, length = 0x000FF8 /* Uncomment for F28374D, F28376D devices */ // RAMGS11_RSVD : origin = 0x017FF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ RAMGS11 : origin = 0x017000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS12 : origin = 0x018000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS13 : origin = 0x019000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS14 : origin = 0x01A000, length = 0x001000 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ RAMGS15 : origin = 0x01B000, length = 0x000FF8 /* Only Available on F28379D, F28377D, F28375D devices. Remove line on other devices. */ // RAMGS15_RSVD : origin = 0x01BFF8, length = 0x000008 /* Reserve and do not use for code as per the errata advisory "Memory: Prefetching Beyond Valid Memory" */ /* Only on F28379D, F28377D, F28375D devices. Remove line on other devices. */ EMIF1_CS0n : origin = 0x80000000, length = 0x10000000 EMIF1_CS2n : origin = 0x00100000, length = 0x00200000 EMIF1_CS3n : origin = 0x00300000, length = 0x00080000 EMIF1_CS4n : origin = 0x00380000, length = 0x00060000 EMIF2_CS0n : origin = 0x90000000, length = 0x10000000 EMIF2_CS2n : origin = 0x00002000, length = 0x00001000 CANA_MSG_RAM : origin = 0x049000, length = 0x000800 CANB_MSG_RAM : origin = 0x04B000, length = 0x000800 CLA1_MSGRAMLOW : origin = 0x001480, length = 0x000080 CLA1_MSGRAMHIGH : origin = 0x001500, length = 0x000080 CPU2TOCPU1RAM : origin = 0x03F800, length = 0x000400 CPU1TOCPU2RAM : origin = 0x03FC00, length = 0x000400 } SECTIONS { codestart : > BEGIN, PAGE = 0 .text : >> RAMD0 | RAMD1 | RAMLS4_5, PAGE = 0 .cinit : > RAMM0, PAGE = 0 .switch : > RAMM0, PAGE = 0 .reset : > RESET, PAGE = 0, TYPE = DSECT /* not used, */ .stack : > RAMM1, PAGE = 1 #if defined(__TI_EABI__) .bss : > RAMLS2, PAGE = 1 .bss:output : > RAMLS2, PAGE = 1 .init_array : > RAMM0, PAGE = 0 .const : > RAMLS3, PAGE = 1 .data : > RAMLS3, PAGE = 1 .sysmem : > RAMLS3, PAGE = 1 #else .pinit : > RAMM0, PAGE = 0 .ebss : > RAMLS2, PAGE = 1 .econst : > RAMLS3, PAGE = 1 .esysmem : > RAMLS3, PAGE = 1 #endif Filter_RegsFile : > RAMGS0, PAGE = 1 .em1_cs0 : > EMIF1_CS0n, PAGE = 1 .em1_cs2 : > EMIF1_CS2n, PAGE = 1 .em1_cs3 : > EMIF1_CS3n, PAGE = 1 .em1_cs4 : > EMIF1_CS4n, PAGE = 1 .em2_cs0 : > EMIF2_CS0n, PAGE = 1 .em2_cs2 : > EMIF2_CS2n, PAGE = 1 /* CLA specific sections */ Cla1Prog : > RAMLS4_5, PAGE=0 CLADataLS0 : > RAMLS0, PAGE=1 CLADataLS1 : > RAMLS1, PAGE=1 EPWM_INT_ISR : > EPWM1ISR_LS0, PAGE = 1 ECAP1_ISR : > ECAP1ISR_LS0, PAGE = 1 CPU2toCPU1_IPC1 : > RAMLS3, PAGE = 1 Cla1ToCpuMsgRAM : > CLA1_MSGRAMLOW, PAGE = 1 CpuToCla1MsgRAM : > CLA1_MSGRAMHIGH, PAGE = 1 /* The following section definition are for SDFM examples */ Filter1_RegsFile : > RAMGS1, PAGE = 1, fill=0x1111 Filter2_RegsFile : > RAMGS2, PAGE = 1, fill=0x2222 Filter3_RegsFile : > RAMGS3, PAGE = 1, fill=0x3333 Filter4_RegsFile : > RAMGS4, PAGE = 1, fill=0x4444 #ifdef __TI_COMPILER_VERSION__ #if __TI_COMPILER_VERSION__ >= 15009000 .TI.ramfunc : {} > RAMM0, PAGE = 0 #else ramfuncs : > RAMM0 PAGE = 0 #endif #endif #ifdef CLA_C /* CLA C compiler sections */ // // Must be allocated to memory the CLA has write access to // CLAscratch : { *.obj(CLAscratch) . += CLA_SCRATCHPAD_SIZE; *.obj(CLAscratch_end) } > RAMLS1, PAGE = 1 .scratchpad : > RAMLS1, PAGE = 1 .bss_cla : > RAMLS1, PAGE = 1 .const_cla : > RAMLS1, PAGE = 1 #endif //CLA_C GROUP : > CPU1TOCPU2RAM, PAGE = 1 { PUTBUFFER PUTWRITEIDX GETREADIDX } GROUP : > CPU2TOCPU1RAM, PAGE = 1 { GETBUFFER : TYPE = DSECT GETWRITEIDX : TYPE = DSECT PUTREADIDX : TYPE = DSECT } }
2. Even though I am using CLA library, Should I also include CLA assembly source file into my project?
3. When I add "CLAsin.asm" source file, it atomatically shows error to add "CLAeabi.asm" but I am working in COFF output format. Help on that