Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

F28M35H22C: RAM_init problem of RAM_BOOT

Part Number: F28M35H22C

Dear team:

One of my customers has a question after referring to the TRM (spruH22i) page 617 routine of the chip:

Can IPC MTOC transfer data into RAM M0 and M1 before C2000 booting?

Best Regards

  • Green,

    I believe this should be OK so long as the RAMs are initialized to 0 first(to avoid ECC errors).  There is a note that the M0 will get initialized to 0 by the C2000 Boot ROM, to the customer could write to M0 before the IPC RAM init referenced in the code above.

    It would probably simpler to just init the M1 and then write both though.

    Best,
    Matthew