Hi I am working with ADC and DAC in Control Card,
I enabled an ADC SOC via software triggering at every 10us. I gave input of shifted sine wave with amplitude 3.3V from a waveform generator.
Now ,To reproduce the waveform through DAC, I Made the result of ADCRESULT register as an Input to DAC via DACVALS Register as shown below (Note: Both ADC and DAC are in 12 bit mode and AQPS = 75ns (Tried with greater than 75ns also))
DacbRegs.DACVALS.bit.DACVALS = AdcaResultRegs.ADCRESULT0;
But My Output from DAC is gets saturated at the peak of the waveform in same amplitude nearly 3.36V as shown below
My Input Waveform for ADC from waveform generator is given below