This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDM-02008: Dimensions of TMDSCNCD280049C

Part Number: TIDM-02008
Other Parts Discussed in Thread: TMDSCNCD280049C, , C2000WARE

Hey Team,

In reference to the TIDM-02008, do we have a spec sheet to show the dimensions for the “J600 C200 MCU control card” also known as TMDSCNCD280049C?

I have an engineer trying to make a CAD model of the circuit.

Best,
Dajon McGill

  • Dajon,

    There should be no need to recreate the CAD model from scratch. The schematic, layout, and all other design files including a 3D model have been included for TMDSCNCD280049C.

    This can be found in C2000Ware at the following link:

    C:\ti\c2000\C2000Ware_3_03_00_00\boards\controlCARDs\TMDSCNCD280049C\A 

    To roughly answer your question though, the dimensions are approximately: 

    2.205" H x 2.647" W x 0.25" D

    Regards,
    Cody