Part Number: TMS320F28379D
Hello,
I have problems with ti-cgt-c2000_20.2.3.LTS compiler.
If optimization level of the project is set to 0 or no optimization is used then there are NO warnings. If I set the optimization level to 1 then I have the following warning:
Description Resource Path Location Type
[W9999] Register write access is in the delay slot of a write of the same register line 191 C/C++ Problem
In attachments, you can find .pp file as described in the article How to Submit a Compiler Test Case.
Thank you in advance!Euler2OmegaInstr.pp.txt