Hi,
Few doubts about ADC and APWM.
1) For a specific ADC module, when is the right point to read the result registers? ADC ISR is not used, as application request. Customer want to use PWM to trigger the SOC with 8KHz, and read the result registers with 5KHz frequency. There's a possibility, during reading, the conversion is in progress. Will bad values be read?
2) For a specific ADC module, 6 input channels. 3 channels are used with 8KHz SOC from PWM, can other 3 be used with 5KHz SOC from software trigger? No ADC ISR is needed.
3) APWM, is there any way to trigger ADC SOC? APWM can be sync with PWM, and PWM can trigger ADC SOC. Beside it, any other ways? Can Timer be used to sync with APWM and PWM?
Thanks a lot.
Br, Jordan