Other Parts Discussed in Thread: C2000WARE
Hi Team
Good day!
Our customer is using TMS320F28035 for measuring Analog channels and sending it through UART. His input is having some offset at ADC input, which is varying from one hardware to another and he dont have provision to control/adjust the offset values in the hardware. In order to resolve the issue, He would like to check the offset value prior through calibration mode and store the values. The ADC values needs to be multiplied and sent through UART. He would like to update this multiplication factor as well. He is able to calculate the offset value and multiplication value. However this process is required to be done at every power ON, which is not desired. He want to do one time calibration for offset and multiplication and store values in microcontroller memory. As this controller(TMS320F28035) does not have EEPROM, using FLASH memory is the only option. Kindly suggest with the sample code or application note to write/read data into the FLASH memory through C code.
BR,
Leon.liu