Part Number: TMS320F28027F
Other Parts Discussed in Thread: LAUNCHXL-F28027F
My development board is LAUNCHXL-F28027F + BOOSTXL-DRV83
I use lab4 torque control to adjust the torque. I gave the value of IqRef_A 0.2. The motor started to rotate. I saw that the current was about 0.3A and the speed displayed by the Speed_krpm variable was about 1600rpm. When I touched the rotor of the motor with my hand At that time, it stopped easily. At this time, the current became 0.10A. Why is the motor weak? Can I stop it easily? How can I adjust it? To generate relative resistance?