Other Parts Discussed in Thread: MOTORWARE, TMS320F28069F
We are seeing poor behavior with MotorWare projects being built in the latest CCSv5.5. We have already tracked one issue down to a build options level difference from 5.4 to 5.5 (which causes projects not to build thankfully) but there are other issues happening where the projects build successfully yet the performance is quite poor (motor doesn't start-up, ID doesn't work, currents look terrible). Sometimes it's dramatic, sometimes you may not notice.
Please do NOT use Compiler 6.2.0, 6.2.1, or 6.2.2 until this is resovled.
Please revert to the MotorWare tested Compiler 6.1.5, and if possible back to CCS5.4.0
Our hope is we are able to patch the MotorWare projects so that they work correctly with 5.5/6.2.1 for the next release (Version _10 in November).