Other Parts Discussed in Thread: MOTORWARE
Hello,
I am controlling AC induction motor in sensorless FOC mode. Controller used in this project is 069Motion. During running there is no load to motor and motor terminal current at 350rpm and 1000rpm as shown in attach file. Especially at higher speeds motor current is not in sinusoidal form. What can be rason of this? Does no load running of AC Induction motor cause this current waveform? I check FOC controller reference and feedback values. Id refefernce=0 so Id_fbk value tracks Id_rated value. Because of no load Iq ref value nearly zero and fdb value tracks reference. And no saturation occurs at PID controllers.
Second question is about estimating flux and Rs value during Lab2a. Estimation controller find estimated flux and Rs value lower than they should be. As an example flux value should be (0.81x 220VAC / 50)=3.56 but algortim finds nearly 2.2. Rs value should be 7.4ohm but algoritm finds 3.5 ohm. What can be reason of this?
Best Regards,
8688.AC Induction Motor Terminal Current- No Load 1000rpm-350rpm.docx