As has been communicated, MotorWare versions up through 1_01_00_11, as well as the InstaSPIN-FOC and InstaSPIN-MOTION GUIs rarely identify induction motor parameters correctly.
This has been solved and fixed internally and will be released in MotorWare _12 at the end of February.
*** Note, there are no plans to update the GUIs. You must use MotorWare projects for ACI motors. If you would like to instrument the variables you can use the UNIVERSAL MotorWare GUI ***
In the meantime, if you have a datasheet (or typically even the nameplate on most ACI motors) you can convert these values into the values required in user.h for Induction motors.
The following posts will show you how. This will also be included in updated documentation for MotorWare _12.