Other Parts Discussed in Thread: DRV8312, CONTROLSUITE
The DRV8312 Evaluation board provides the three current feedback channels to the control card interface on two seperate ADC pins totaling 6 channels, but the InstaSpin firmware sets up the ADC to only convert one of the two pairs of inputs for a total of 3 channels actually used. What is the reason for providing two identical channels if they are not used?
I ask this because in duplicating the design, we would like to do away with the duplicated channels so we can use the ADC channels that are freed up for other system analog. As long as we keep the channels that are needed by the InstaSpin code can we safely remove the duplicated channels?