Hi;
I am using;
tms320f28027f, c2000 launchpad with a maxon bldc motor and drv8301 motor drive.
I am confused as to which method is the best method to produce an electric generator!
Using the InstaSPIN Universal GUI, I am able to vary the Iq_Ref.
By setting this to a negative value, I can demand an arbitrary negative value of current, which- according to a 4-quadrants of operation- should generate electricity via the back EMF.
Indeed this is true, I have coupled the two motors I am using, and can confirm that the generator device (hardware stated above) is generating electricity. The amount of back EMF is also increased by increasing the magnitude of the negative current, although I am not aware of the equation that would define this relationship, can I have the direction to such resource please?
This generator will be used in a dynamic system, I am not sure if the Iq_Ref should vary (inverse) proportionally with the speed of the driving motor?
I know that this can be configured in CCS however, after speaking with some colleagues, they have suggested trying to altering the PWM output, directly in the project (project11)!
My main question is;
Which method is the best/correct in order to produce a generator (not a regenerative braking system);
through the current controller?
or
by modifying the PWM structure (using the example given in the "HAL Module of MotorWare" document)?
Kind Regards
Morikeh