Other Parts Discussed in Thread: DRV8305
Tool/software: Starterware
Hi,
I am trying to use TMS320F28069M launchpad and DRV8305 booster pack to run foc on my hobby grade motor, in order to replace my old bldc motor controller. However, except for the low noise at low speed range, foc performs significantly worse than bldc. I wonder if I did anything incorrectly?
I'm using sunnsky x2814-900KV motor. All the PI control parameters are calculated by default in the labs.
1. FOC generated way less torque than BLDC. For example, at low speed, I can stop the motor under foc with my hand easily at around 1.5A supplying current. But stopping the motor under bldc control is much harder-the motor draws over 10A before it comes to a full stop.
2. FOC creates a loud and high pitch noise at around 4000rpm but the noise disappear when further increase the speed. This problem does not appear on bldc control so I don't think it's the motor problem.
3. At 0 speed, FOC create a noticeable white noise in the motor but this is not the case in bldc control.
I've changed R8,9,10,14 to 22kohm and C10,11,12,22 to 0.031uF to allow better filtering and sensing. Here's my configuration:
#define USER_VOLTAGE_FILTER_POLE_Hz (1185.73) // 1/(2*pi*(R14*R16)/(R14+R16)*C22) #define USER_PWM_FREQ_kHz (45.0) #define USER_IQ_FULL_SCALE_FREQ_Hz (1501.5) #define USER_IQ_FULL_SCALE_VOLTAGE_V (13.0) #define USER_ADC_FULL_SCALE_VOLTAGE_V (17.85) #define USER_IQ_FULL_SCALE_CURRENT_A (25.0) #define USER_ADC_FULL_SCALE_CURRENT_A (47.14)
I would really really appreciate if anyone can shine any lights on this?
Thanks!
Xunjie