Part Number: INSTASPINUNIVERSALGUI
Hi
I have the high voltage Instaspin evaluation kit, yellow board, black housing. It comes with two controllers, F2802 and F2806_ISO, Ive use the F2806 for the GUI_Composer_Instaspin program, seems to run ok. I want to also run the HVMTRPFC motor GUI, which control card do I use.
If I want to run the labs program, again which control card do I use. Why 2 cards, the F2802 has no USB connections.
Thanks
Thomas