This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSHVMTRPFCKIT Problem with HVMTRPFCKIT-GUIv1.exe

Hi team,

I have a problem with the  GUI xxx, I installed correctly the driver USB on my PC as request the system.
I verified the presence on my pc of Microsoft .NET framework 2.0 or higher and there are.
well, when i run the programm I set the serial com at 57600 and I connected my pc with the kit correctly, led green on on the GUI but the programm show me this:

Then I press "Continue",  now the programm doesn't allow select the motor but if I push the button start stop, the motor turn on / turn off.

When the motor is turned on and I try to move the  cursor  for the Speed Reference another Message is showed:

 

 Please, Could Help me.... there's a new sw for the GUI or new Firmware for the KIT.

Thank a lot

Pierluigi Rossetti