Hi, Experts,
I'd like to know how the F28335's DMA pipeline (illustrated in Figure 3 on SPRUFB8D) changes when DMA source and/or destination is XINTF.
For instance, with a XINTF zone configured with Lead/Active/Tail timing being 1/3/1 (XTIMCLK=SYSCLK), and use this as DMA source, then "Read SRC data" cycle in the diagram (which takes 2 cycles on the fiture) replaces 5 cycles? Or it becomes 6 cycles? How about the case when such XINTF is set to DMA destination?