Other Parts Discussed in Thread: CCSTUDIO, CONTROLSUITE, SPRCAA6
I am looking for the FlashAPIInterface2802xV2_01.out to be used within a stand alone Flashburn utility.
However it seems that the current mechanism to deliver updates is either broken or misdirected.
In the past in order to obtain a Flash Agent API, it would be available within
a. CCS Algorithm Directory (i.e. C:\CCStudio_v3.3\plugins\Flash28xx\Algorithms\ or C:\Program Files\Texas Instruments\ccsv4\C2000\flashAlgorithms ...)
b. Via a download link organize on this link
http://www.ti.com/mcu/docs/mcudevtoolsandsw.tsp?sectionId=96&tabId=1503&familyId=916&toolTypeId=11&go=Go
However Current documentation for newer devices,which require newer FlashAPIInterface version as they are Silicon Revision A, refers the end user to the ControlSUITE Package
(http://www.ti.com/tool/sprc848, http://www.ti.com/tool/sprcaa6)
In controlSUITE there are only examples for the API integration (Example_Flash2802x_API.out), and does not have the General LIB Flash Agent.
Where can I get the new FlashAPIInterface agents for 2802x0, 280200 devices?