Other Parts Discussed in Thread: CCSTUDIO
Hi Everyone,
I am using a F28335 processor, and am trying to setup the FFT libraries downloaded from sprc081. The issue I'm having is when compiling the code, I receive the following error.
The specific code I am trying to build is located in fft\cstb\fft128r\build, however I've received the same error on each included project, regardless of the .cmd and .map files I have included. Has anybody came across a solution to this error or know where the Tag_Memory_Model attribute value is specified?
----------------------------- build.pjt - Debug -----------------------------
[Linking...] "C:\Program Files\Texas Instruments\C2000 Code Generation Tools 5.2.1\bin\cl2000" -@"Debug.lkf"
<Linking>
fatal error: file
"C:\\tidcs\\c28\\dsp_tbox\\fft\\cstb\\fft128r\\build\\Debug\\fftrd.obj" has
a Tag_Memory_Model attribute value of "2" that is different than one
previously seen ("1"); combining incompatible files