This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can Flash API v2.01a be used on 2802x Rev 0?

Is it possible to use the Flash API v2.01a on a 2802x Rev 0 if I use it in software mode?  The notes for v2.01a specifically say on page 4: "These release notes apply for only TMS320F2802x Rev A and doesn't apply for TMS320F2802x Rev 0..." but why couldn't the v2.01a be usable with the software library (Flash2802x_API_V201.lib)?  I'm thinking the documentation wasn't completely updated between v2.01 and v2.01a.  In fact, this same page of the document references Flash2802x_API_V200.lib instead of V201.lib...

Along the same lines, what really changed between V2.00 and v2.01?  Both are listed as initial releases.  From a cursory glance:

2.00: Software Only

2.01: Boot ROM Rev A only

2.01a: Boot ROM Rev A or Software