Hello,
I have an application (for an AC/DC power supply) with a Piccolo F28035.
The product is now in production and I have a lot a pieces rejected due to a calibration out of range.
After investigation, it appears that the ADC of some Piccolo devices are very very non linear
I plotted the curves for 2 boards (same software, same production batch) and they are very different (one is pefectly linear, the other one has large steps as if the ADC was only 8 or 10 bits).
Has this problem already been observed ?
A second point : I'm using an external ref (3V) and I try to change the settings of the AD conversion to investigate on the AD linearity problem.
At 2.3V I read 3140 for the converted value (this is 2.3*4096/3, so this is correct).
Then I change the software to use the internal reference ( AdcRegs.ADCCTL1.bit.ADCREFSEL = 0; )
At 2.3V, I read 3350. It should be around 2.3x4096/3.3 = 2850.
Why ???
Best regards