Other Parts Discussed in Thread: TMS320F28027
Hi Folks
I have an application with 3 TMS320F28027 (Slaves) and 1 ARM Cortex M3 (Master) Processor. For measurement reasons, it is critical, that the 3 Slaves run on a synchronized clock. The Piccolos are using their internal oscillators - no external crystal available. I would like to modulate the sync signal for the slaves onto an existing signal, since I have galvanic isolation between master and slaves. I made some tests catching the sync pulse with a trip zone input triggering an interrupt , which worked fine. The problem I face now is how to trim the internal oscillator. Does anybody know an easy an fast algorithm to find the correct settings for the INTOSCnTRIM register?
BR Andreas