Does anyone know if there is an opensource tool for coding for the TMS320LF240[67] series 16-bit fixed-point DSP ICs. These DSPs have quite respectable ADCs in them, and I'm curious to do some experimentations with one as part of a software defined radio receiver. Maybe other experiments too.
At my work I use CodeComposer on Windows to develop for the '2406A, which while not bad, isn't quite my preference in terms of IDE (I'm used to vim, make and Insight/gdb on Linux) it's quite usable. At home however... I do not have a computer running Windows, and can't afford the steep cost of CodeComposer. (Remember, I'm an individual doing it as a hobby, not a company doing it as a business.)
I've heard of some ports of the GNU toolchain to some of the more modern DSPs, but was wondering if anyone had seen any tools for the 2406 and 2407? Something opensource would be desirable as not all my development systems are i386 compatible (the one I use for Stellaris development is MIPS), and it does mean I have the option of looking at fixing problems myself if I encounter them (as opposed to being reduced to just making bug reports).