This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

two codestart in CMD file



Hi, all.

           I am using F28035.

           In the normal cmd file:

           BEGIN               : origin = 0x3F7FF6, length = 0x000002

           codestart          : > BEGIN       PAGE = 0

           Now, I want to change the BEGIN section to : origin = 0x3E8000, length = 0x000002.

           But after the chip power on, the app do not run.

           So, I think no matter  what  address asign to BEGIN, the chip will start at 0x3F7FF6, am I right?

           and how can I asign the codestart section to two place, (eg 0x3E8000 and 0x3F7FF6 have the same data), what should I do?

            

           Best Regards,

           Edwin