Hi,
I've used my TMDS320F28335 experimenter kit without any issues until the control card which is cased on the 'experimenter's kit USB docking station' have got the leds switched off at the same time the CCS_v6 wasn't able to recognize the target and connect to it anymore. Only the USB port was used for the tests and no inputs were connected in GPIO's. All the configs and drivers were reviewed, the device tested on other computers and no sucess. The board's green led lights while the control card's leds remain off. They used to light as soon as the device was switched on. Now, as you can presume, the connection test in target configuration, results in 'failure test'. I guess it is more hardware problem.
What can I do?