Other Parts Discussed in Thread: TMDSHVMTRINSPIN
hi,
i designed and make a pcb based on a hvkit_rev1p1(with a few differences) but with F28027 MCU, for driving a 0.75hp ACIM, 220v, 3 phase motor and i am using a CCS6.1 and motorware15.
the max speed of the motor is 1.5krpm. the motor receive to this speed when rotating in NO Load state. but when the load apply to motor, the speed decrease (to about 1.1krpm) and doesn't go to max speed. in the other word, i am driving the motor with maximum 65% efficiency but i expected to receive to 80%.
i tried this experiment with dynamo-meter and can't reach to 2.5Nm in torque. i tried to solve this problem but i can't.
also i tired to increase the MAX_CURRENT to catch more speed but i can't.
where is the problem? is this natural or not?
is there anyone to help me to solve this problem and reach to desire speed with Load?
this is my user.h file: