Part Number: TMS320F28069
Hi,
I am using TMS320F28069. Following are my observation :
Schematic Points
Vref hi = Open (No voltage impressed)- internal reference is used.
Vref lo = 0 Volts
VDDA = 3.3V
| S/n | Voltage (Volts) | Digital Count Received in ADC | Expected count | Difference |
| 1 | 0 | 4 | 0 | -4.00 |
| 2 | 0.5 | 671 | 620.45 | -50.55 |
| 3 | 1 | 1256 | 1240.91 | -15.09 |
| 4 | 1.5 | 1830 | 1861.36 | 31.36 |
| 5 | 2 | 2459 | 2481.82 | 22.82 |
| 6 | 2.5 | 3012 | 3102.27 | 90.27 |
| 7 | 3 | 3533 | 3722.73 | 189.73 |
Digital Count which I am expecting for a particular voltage = (Voltage*4095)/3.3
But as you can see in the table the difference in count exceeds as the voltage is increased. This is causing error in my readings.
Kindly suggest what can I do to reduce this difference in readings.
Regards,
Siddharth Gupta