This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28075: EPWM1 module of 100pin chip

Part Number: TMS320F28075

Tool/software: Code Composer Studio

Part of the previous questions has been solved by myself, but still have issues about the EPWM timing. So, I modified the questions as follows. Sorry for the inconvenience!

I am using the 100pin 28075 chip right now. Since the EPWM1 module is not pined out in this version, I tested to use EPWM7 module instead. The SYNCIN source is EXTSYNCIN1 by configuring SyncSocRegs.SYNCSELECT.bit.EPWM7SYNCIN = 5. But the delay between the rising edge of EXTSYNCIN1 and EPWM7A sets is 80ns. Why the delay time is so long? The EPWM clock frequency is 100MHz.

I have used TMS320F28027 before with 60MHz clock frequency in the same way, and the delay time is 70-90ns. So, I feel maybe something is wrong? or the propagation delay of muxes circled out in the figure below is too long? Where can I find the propagation delay information of the muxes circled out in the following picture?

The code is attached below for your convenience. Thank you in advance!

5531.28075_TEST_EPWM_EXTSYNC.zip