Part Number: TMS320F28377D
Hello everyone,
I'm using the TMS320F28377D microcontroller, and in my project I have current sensors and voltage sensors. Each sensor can output a voltage from 0 to 5V (depending on the measured parameter), however, I designed my project such that the maximum measured currents or voltages are associated with sensor output voltage less than 3.3V.
The problem is that I get transient overshoots (up to 4.5V) in the sensor output voltage ... I haven't interfaced the sensors to the microcontroller yet. Do I need to add a protection circuit to clamp these transient overshoots or the microcontroller has a built-in protection and won't be harmed by these overshoots?
Thanks,
Nour