Part Number: DRV8301-69M-KIT
Other Parts Discussed in Thread: DRV8301, MOTORWARE
Hello,
I am trying to generate debug outputs that can be measured via oscilloscope. I want to be able to output variables internal to the controller, such as commanded torque.
I would like to do this in realtime, so that the values can be correlated with measurements from external sensors.
Does the DRV8301-69M-KIT have any additional analog outputs (DACs or PWMs with lowpass filters) that are exposed somewhere on the board, and aren't already utilized during operation of a BLDC?
It appears another user was doing something similar in this thread, although there was an unanswered question about transferring the code to DRV8301: https://e2e.ti.com/support/microcontrollers/c2000/f/902/p/469498/2088061#2088061
Could someone point me in the right direction for modifying one of the existing motorware labs to enable a PWM output if possible?
Thank you,
Max