Hey
The code provided by TI, does it have an option to set the reference real power setpoint for the inverter? I know the development kit is rated for 500W, but if I want it to produce 200W does the code allow me to do so?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey
The code provided by TI, does it have an option to set the reference real power setpoint for the inverter? I know the development kit is rated for 500W, but if I want it to produce 200W does the code allow me to do so?
Shammya,
Please refer to the UG of those kits,
As these are MPPT based design, they will pump as much power the panel is able to provide, or close to the MPPT point.
I am unaware if there is specific function out of the box that limits power as you mentioned.
Rest, everything is in the code for which the source code if available to you, so you should be able to implement any new functions.
Regards
Manish Bhardwaj