Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LVBLDCMTR: Somebody know LVBLDCMTR + Hall sensor + Encoder(1024) information?

Part Number: LVBLDCMTR
Other Parts Discussed in Thread: LVSERVOMTR, 2MTR-DYNO

Dear TI

I ordered five LVDCMTR products new days ago. then it is a motor for Sensorless Application!(non hall sensor

cable and i don't find addition information product in telcointercon homepage.)

I want to know where to buy LVDCMTR + hall sensor + encoder(1024) interface(manufacturer order name and so on).

or  would like to know other homepage (or a seller) about the bldc motor products including Hall sensors and encoders.

I am in need for a test motor to develop an application that uses Hall sensors and encoders!!!

Best regards

이메일에 긍정적인 답변을 주신분에게 신의 축복이 있기를!

  • we include a similar motor with hall sensors in the DRV8312-C2-KIT and DRV8312-69M-KIT but we don't sell this one individually.

    What we do sell is LVSERVOMTR which includes encoder and hall sensors. We include two of these are part of 2MTR-DYNO with shaft connectors and a frame mount for doing active load testing.

    Otherwise there are hundreds of companies who will sell motors, but they often have minimum quantities.  You should find someone local if you go this route.

  • Dear ChrisClearman

    I am not an expert in the field of motors. I have one question.The recommended motor is PMSM motor + Hall sensor + encoder.
    Can the PMSM motor be used like a BLDC motor? I wonder if there is only difference of motor control method.

    Best Regards. 당신은 축복받을겁니다. 감사합니다.
  • yes, only difference is in chosen control method. You can drive them with 6-step trapezoidal or sinewave/SVPWM/FOC.

    both motors are sinusoidally wound permanent magnet machines.
  • Dear ChrisClearman

    I wanted to be sure about the control method.

    Thanks you~!

    Warm regards.