Other Parts Discussed in Thread: LAUNCHXL-F280049C, , TMS320F28075, LAUNCHXL-F28379D, TMDSDOCK28379D
For a new project we need a T.I. DSP with 2* I2C bus (and SPI and enough memory). For this project we prefer the TMS320F28xx series.The two I2C busses are needed for reading pressure sensors with I2C interface (for controlling pumps) so the 2 busses will have the same functionality here. These sensors require a standard I2C interface and are not individually adressable. When I look in the overview of the TMS320F28xx series there are 2 possible candidates with 2* I2C bus:
- TMS320F28004x
- TMS320F2807x
However the TMS320F28004x has 1* I2C and 1*PMBUS.
So what would you suggest here? Can we use the PMBUS in the same way as I2C or are there any software issues when using this bus for I2C?
The TMS320F28004x looks something cheaper but some suppliers here in Europe (like EBV/AVNET) does not have them at stock at this moment and we want to be sure that we don't get problems with stock the next months.
And are there evaluation kits available for these processors?
Regards
Chris van der Aar
NTS Systems Development
Eindhoven , The Netherlands