Hi
We have a product on the market which works nicely at room temperature, but if it is switched off at elevated temperatures it wont switch on again until it cools down.
It is set up to boot in GetMode. I have scoped the TDO, GPIO34, TRST and XRS pins during startup, and they seem to do as expected.
I tested here in a chamber at 55 degrees, where the boot fails, but once it is back at room temperature it works again.
The specific chip I have here is F28069UPZPS, G4 A-6BC19QW, so it is an A revision.
I saw in the erratas an issue with the internal oscillator affecting CAN bootloading at high temperatures. Could it be that there is a similar issue here?
I hope someone can help.