This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28379D: USB cable connection - EMI

Part Number: TMS320F28379D

Tool/software: Code Composer Studio

Hello everyone,

Today I was conducting some experiments with an inverter that generates EMI noise. 

I was using the conventional USB cable that comes with the TI control card to connect with the DSP. Everything works fine until a certain current level above which I lost the connection with the DSP. I highly believe the problem is caused by EMI of the inverter.

The TMS320F28379D already have an isolation for the USB so I dont need another one, right?

Have anyone faced simmilar issues? Does anyone know if is there any special type of USB cable that can reduce the problem? Are the USB cables that comes with the control card shielded? Does it make any difference? Should I try to shield them?

I will try to find the answers and if I figure it out I will post here the solution. Meanwhile, I appreciate any help.

Thank you,

Renato