Hi community
I have following question:
In the initialization of the ADC from the derivate TMS320F2812 I recognized that the Bit ADCTRL3.EXTREF is set to 1 (means the ADC reference works with the external voltage source) (image "Register ADCTRL.jpg").
The Pins for the external reference voltage source "ADCREFP" and "ADCREFM" are connected like in the image "ADC Pin Conn with internal reference.jpg".
Now my question is, how the analog to digital conversion works correctly without a external reference voltag source? So what happens, when the ADCTRL3.EXTREF is set to 1 and no external reference voltage source is connected? Is this allowed?
In the image "ADC Pin Conn with internal reference.jpg" in the section "Note:" is just the case described, if an external reference voltage source is connected and the bit ADCTRL3.EXTREF is set to 0.
Thanks for your help.