Other Parts Discussed in Thread: UCD7138, CONTROLSUITE, UCD3138A
Hi all
We are using the TIDM-1001 eval board for evaluating our custom hardware setup. For this we started with the 283779D source code contained in controlSUITE. This works well and therefore we are going further. On the eval board the UCD7138 are mounted and the 4 DCT signals are routed to the 28379D (GPIO 11,13,14,20). Unfortunately those 4 pins are not used by the source code I have.
Is there source code around which does the functionality stated in the doc (bold highlighted part)?
The documentation TIDUCT9 states in section1.6.5 SR PWM Drivers:
"... Four of these drivers are used to drive the four SR switches. This approach brings a huge performance or cost benefit to the system as no other type of additional, and usually dissipative, current or voltage sensing is required to determine this accurate turnon instant for the SR switches. The SR turnoff instant is controlled by the C2000 MCU."
Thank you very much and best regards
Roger