Other Parts Discussed in Thread: TMDSCNCD28335, , TMS320F28335
Tool/software: Code Composer Studio
I was trying to connect my TMDSPREX28335 kit to my hardware experiment. So I dumped my program on to the kit via CCSV4, after dumping the program I took the kit and connected a 5V supply and tried to connect to my hardware setup but eventually was not able to get any signal out of the kit. So I tried again to dump the program on the kit again but this time I am unable to connect it to the CCV4 and the following error is displayed also the tms320f28835 chip on tmdscncd28335 card is getting very hot on connecting to the laptop.
the value is '-151' (0xffffff69).
The title is 'SC_ERR_FTDI_OPEN'.
The explanation is:
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.