This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/TMS320F28069: Where can I find a CCS target configuration file for TMDSCNCD28069ISO control card?

Part Number: TMS320F28069
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28069ISO

Tool/software: Code Composer Studio

We need a target configuration file for using TMDSCNCD28069ISO control card with CCS.  We can’t seem to make one that works.  The C2000Ware examples don’t have one in them that works, at least with our board.  

  • Note that the standard controlCARD target config file from C2000Ware will work with TMDSCNCD28069ISO, but the confusing part is which USB port to plug into the PC.

    You need to connect a USB cable from the PC over to the J1 connector of the TMDSCNCD28069ISO. Then you also need to provide power to the dock, but if you also plug the dock into your PC it enumerates as a second XDS100, causing confusion for CCS.

    The easiest solution is to power the dock using an external USB 5V power source connected to (JP2) of the dock or use a 5V wall wort with barrel connector at (JP1) of the dock. This way only a single XDS100 connection is made to the PC from J1 of the TMDSCNCD28069ISO.
  • Thanks for root causing this Ruben, I hadn't thought about the 2nd XDS100 enumerating in terms of causing a question when starting CCS. I'll see if there is something we can clarify in the Infosheet/getting started.

    Best,
    Matthew