Part Number: TMS320F28069
Dear Sir,
I am currently working on the TMS based experimenter kit to control the Switched reluctance motor . Many things i experimented . I would like to go for my actual board design. I need to actuate the SRM motor of 2A capacity. Which series of micro controller is best suitable for this. I need to do position sensing of inductor based on capture model . PWM actuation is to be done based on the position sensing .I am going to start my new design. I should select a controller which should be available in the market for long time . kindly suggest a good part and the reference design also pl. this is for automotive suspension system based on SRM control.
Kindly suggest me the suitable SRM Gate drive as well as MOSFET circuitry to do the job also.
Thanking you,
Warm Regards,
S.M.Sundari