This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D: Symmetrical complementary PWM outputs with HR and deadband

Part Number: TMS320F28377D
Other Parts Discussed in Thread: C2000WARE

Can F2837xD devices produce symmetrical complementary PWM signals with high resolution and deadband? I've managed to configure micro to produce symmetrical complementary signals (e.g. for 3 x 2 signals for 3 phase motor control), but I can't achieve high resolution whilst maintaining symmetry. In this setup, the HR sub block needs to be configured to apply MEP to both edges, but that results in breaking symmetry when CMPAHR is not 0x80.

Am I missing something?

Thanks,

Viktor