Other Parts Discussed in Thread: C2000WARE
Tool/software: Code Composer Studio
Hi,
F28034 SCI Communication will lost data when transfer 8 bytes, only 5 bytes can be transfer. but the configuration in F28232 is as the same as the F28034, F28232 can send out 8 bytes normally.
why SCI in f28034 can't transfer 8 bytes just as the way F28232 does?
when we add one line of code like this:
while(SciaRegs.SCICTL2.bit.TXEMPTY==0)
the F28034 did send out 8 bytes completely, but it will cost 6 ms delay after adding this code.
is there any difference about the SCI between F28034 and F28232?
//configuration as below
SciaRegs.SCICCR.all =0x0007;
// 1 stop bit, No loopback, No parity,8 bits,async mode,idle-line
SciaRegs.SCIHBAUD = HI_BYTE(BAUDREG);
SciaRegs.SCILBAUD = LO_BYTE(BAUDREG);
SciaRegs.SCICTL1.all =0x0023;
// Relinquish SCI from Reset
SciaRegs.SCICTL1.bit.RXERRINTENA = 0;
SciaRegs.SCICTL1.bit.RXENA= 1;
//SCI enable
SciaRegs.SCICTL1.bit.TXENA= 1;
//0 //SCI transfer enable
SciaRegs.SCICTL2.bit.TXINTENA = 0;
//Enable TXTDY Interrupt
SciaRegs.SCICTL2.bit.RXBKINTENA = 1;
//Enable RXTDY Interrupt
SciaRegs.SCIPRI.bit.FREE = 1;
SciaRegs.SCIFFRX.all = 0xC021;//RX FIFO Enable
SciaRegs.SCIFFTX.all = 0xC000;//TX FIFO Enable,AliCheck C000
SciaRegs.SCIFFCT.all=0x00;//
SciaRegs.SCIPRI.bit.FREE = 1;
SciaRegs.SCICTL1.all =0x0023;
// Relinquish SCI from Reset
//Transfer code
if(SciaRegs.SCICTL2.bit.TXEMPTY && (SciaRegs.SCIFFTX.bit.TXFFST <= 0x00))
{
for(; mbComm.cursor < 8; j++)
{
SciaRegs.SCITXBUF = mbSendBuffer[mbComm.cursor++];
//while(SciaRegs.SCICTL2.bit.TXEMPTY == 0);
if(j >= 15) //16
break;
}
}