Part Number: TMS320F28027
Other Parts Discussed in Thread: CONTROLSUITE, TIDM-HV-1PH-DCAC, MOTORWARE, C2000WARE
In the design of my drive control (sensored FOC) I have reached a very promising point using the F28027 Controller on a custom layout, worth mentioning without InstaSpin – so this is a “classic” F28027 Controller. The mathematical transformations are largely based on the open source software part of InstaSpin and “controlSuite motor app blocks” and delivers as described already good results.
However, the phase current shows a 5th - and 7th harmonic / harmonic wave, which limits the maximum usable power of the system due to a distortion of the current. I assume that TI has already dealt with the issue of "harmonic cancellation" in the field of motor control. I have already found some approaches from the literature dealing with harmonic elimination. Examples would be an AFC controller for harmonics or, as described in reference design TIDM-HV-1PH-DCAC, the use of a 2P2Z - compensator.
Ultimately, I am still at the beginning with my elaborations on this topic.
1. Is there ideally source code specifically for the implementation in the field of motor control?
2. Should I use a compensator like the one shown in the ref. Design (TIDM-HV-1PH-DCAC), how are the coefficients determined for a harmonic cancellation?
3. TI offers a tuning guide for PID controllers, is there comparable literature for compensators?
4. Are there other approaches to eliminate the harmonics?
I would be delighted to have initiated an interesting discussion here and am looking forward to the exchange.
Best regards Benjamin