Part Number: TMS320F280049C
I need to know what is the use of memcpy function?
On power on it is called as:-
memcpy(&RamfunctionStart,&RamfunctionLoadStart,(size_t)&RamfunctionLoadsize);
RamfunctionStart, RamfunctionLoadStart & RamfunctionLoadsize are declared as 16 bit variables
memcpy function is declared as :-
#pragma CHECK_MISRA("-16.4")
_code_access void *memcpy (void *s1, void *s2, size_t n)
Thanks in advance.
Regards