Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
Hi,
I am using the TMS320F28335 board, and when I put the LED blinking code on the flash and run it after debugging, the LED blinks well.
I want to check the stand alone status, but it doesn't work.
How can I check the led blink with stand alone?
The boot mode is set to jump to flash, and the process of checking the led blinking on the stand alone is as follows.
CCS Shutdown, Board Off, XDS100v2 Cable Remove, XDS100v2 Cable Connection, Board On.
There is no response to the LED.
To power the TMS320F28335, the only option is the XDS100V2 cable.
Thanks, Han