Tool/software: Code Composer Studio
Hello,
I just started using TMDSDOCK28379D with Docking Station. I power up the board with USB cable provided, connected to the Docking Station.
When I try to debug it, I get this error:
</quote> Error connecting to the target:
(Error -151 @ 0x0)
One of the FTDI driver functions used during the connect
returned bad status or an error. The cause may be one or
more of: no XDS100 is plugged in, invalid XDS100 serial number,
blank XDS100 EEPROM, missing FTDI drivers, faulty USB cable.
Use the xds100serial command-line utility in the 'common/uscif'
folder to verify the XDS100 can be located.
(Emulation package 8.3.0.00003)
</endquote>
When I ran the xds100serial command-line uitlity I got "No XDS100 found in the system".
Do you have any suggestions on what I can try next?
Thank you.