This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28069: XDS110: is it possible to bypass VTREF?

Part Number: TMS320F28069


Hello,

I'm working on a project based on a TMS320F28069. We use a tag-connect connection for debugging and thus don't have the VTREF signal on the JTAG link. We only have the following signals:

  • TDI
  • TDO
  • TMS
  • TCK
  • nTRST
  • GND

When connecting the XDS110 debug probe to our PCB, the debug probe raises an error saying that the PCB is not powered which is normal since the VREF signal is not connected to the PCB.

Is there any way to bypass the XDS110 VTREF signal (i.e. setting the configuration of the XDS110) to bypass target board power supply measurement and force the JTAG communication voltage level? If yes, how?

Thank you in advance for your help.

Best regards