Hi,
my customer is using F28033's SPI to communicate with MCP2515.
F28033 is master, SPISTEA connect to CS pin of MCP2515. baud rate is 2M. Customer transmit 3 8-bit data successively.
The good waveform is as below: green-clock, blue-CS pin.
99% the communication is good, but there is low probability that the waveform is as below:
The clock stops in the middle, and CS pin goes high as shown below:
We've no idea why it's like this, any idea?