Part Number: TMS320F280049C
Hi
I have an issue of TMS32F280049C on a 6.6kw OBC project. The update of value in CMPA (EPWM1) is incorrect at line zero cross. CMPA is written by a value approximate 100%, but the duty of PWM from DSP output is approximate 0%. the error is often incidental.
Here are a party of source code and waveform:
1:Waveform
The 4th Channel: DAC output according to variable "PFC_Duty" . It is correct in Red circle position.
The 1st Channel: PWM output according to variable "PFC_Duty" . It is incorrect in Red circle position.
The 2nd Channel: PWM complementary output with 1st channel . It is incorrect in Red circle position.
2. Source code
interrupt void ISR4(void) ----->is called every 14.92us
{
EINT;
Grid_Vols = (float)PFC_V_GRID_ADCREAD - 2505.0f;
Grid_Vols = Grid_Vols * .42228;//.39196; //.4259;//.3; // Scale to real world volts
CLA_forceTasks(CLA1_BASE,CLA_TASKFLAG_2); ----->To trigger task 2 in CLA
....
DAC_Output_Val = (DAC_Output[4]*0.0000152587890625)*5;
DAC_setShadowValue(DACA_BASE, DAC_Output_Val);
} ------>about 5us for this routine
static inline void CLA_TASK2(void)
{
....
cla_temp =(uint32_t)(PFC_Duty*65536.0);
DAC_Output[4]=cla_temp;
HWREG(PFC_LEG1_PWM_BASE + HRPWM_O_CMPA) = cla_temp;
cla_temp = (uint32_t)(PFCDB*65536.0);
HWREG(PFC_LEG1_PWM_BASE + HRPWM_O_DBREDHR) = cla_temp;
HWREG(PFC_LEG1_PWM_BASE + HRPWM_O_DBFEDHR) = cla_temp;
} ------>about 13us for this routine
Please help advise the possibilities. Thanks.